The Test Center offers accredited services to perform Product Safety tests, which are required to show conformity with the Low-voltage directive of the European Union and other regulatory provisions needed on the global markets.
In the case that tests cannot be performed in the Test Center we will organize these tests to be performed by an adequate Test Laboratory.
In addition, the Test Center offers general risk assessments required for special purposes.
Safety Tests for electrical equipment for measurement, control, and laboratory use are performed according to the Standard family IEC 61010
(Safety requirements for electrical equipment for laboratory use - Part 1: General requirements) including their local deviations.
General safety requirements | IEC/EN/CSA/UL 61010-1 |
The equipment und test (EUT) is tested for complying with various requirements considering electrical, mechanical, |
Particular safety requirements for laboratory equipment for the heating of materials | IEC/EN/CSA/UL 61010-2-010 | |
Particular safety requirements for automatic and semiautomatic laboratory equipment for analysis and other purposes |
IEC/EN/CSA 61010-2-081 | |
Particular safety requirements for in vitro diagnostic (IVD) medical equipment | IEC/EN/CSA 61010-2-101 | |
Risk management for medical and IVD equipment | ISO 14971 | Evaluation of the Risk Management required for IVD medical equipment. |