The Test Center test lab is accredited to ISO/IEC 17025 ('General requirements for the competence of testing and calibration laboratories').
The accreditation is certified by DAkkS (Deutsche Akkreditierungsstelle).
The Test Center's quality system is based on a database especially designed and developed for laboratories and it is compliant to ISO/IEC 17025.
The database in use is LDMS (Lab Document Management System).